Skip to main content
Visitor II
September 10, 2025
Solved

Unable to play audio on TAS2110 codec via SAI using STM32U5G9J-DK1 board

  • September 10, 2025
  • 3 replies
  • 971 views

Post edited by ST moderator to be inline with the community rules especially for sharing a code. Please read this post.

I’m working on playing audio on the TAS2110 codec using the STM32U5G9J-DK1 board via SAI.

  • I tested with generated sine and square waves, and I can hear output on the speaker.

  • However, when I try to play audio data stored in memory, I don’t get any sound.

To store the audio file, I created a .s file as shown below:

.section .wav_data, "a"
.global _wav_data
_wav_data:
.incbin "C:/Work/Project/Project/audio_codec/Core/Src/wav/audio.wav"
.global _wav_data_end
_wav_data_end:

I can parse the WAV data using my parser API. Parsing works fine, and I copy the samples into a buffer, then send it to SAI via DMA.

Could you please help me identify what I might be missing? Why do I not get audio output from the speaker when streaming from the WAV file?

My GPDMA and SAI configurations are set up accordingly.

Jinal_0-1757488994988.pngJinal_1-1757489026142.png

Jinal_2-1757489078805.png

Jinal_3-1757489228733.png

Jinal_4-1757489348204.png

In the linker script

.wav_data :
{
. = ALIGN(4);

_swav_data_start = .;

KEEP(*(.wav_data))

_swav_data_end = .;

} >FLASH

 

Parse API

 
int parse_wav_file(uint8_t *wav_data, uint32_t wav_size, wav_info_t *info) {

if (wav_size < 44) return -1; // Too small for header



// Check RIFF header

if (strncmp((char *)wav_data, "RIFF", 4) != 0) return -1;

if (strncmp((char *)(wav_data + 8), "WAVE", 4) != 0) return -1;



// Find fmt chunk

uint32_t offset = 12;

while (offset + 8 < wav_size) {

if (strncmp((char *)(wav_data + offset), "fmt ", 4) == 0) {

break;

}

offset += 8 + *(uint32_t *)(wav_data + offset + 4);

}

if (offset + 8 >= wav_size) return -1;



// Parse fmt chunk

uint16_t audio_format = *(uint16_t *)(wav_data + offset + 8);

info->num_channels = *(uint16_t *)(wav_data + offset + 10);

info->sample_rate = *(uint32_t *)(wav_data + offset + 12);

info->bits_per_sample = *(uint16_t *)(wav_data + offset + 22);

if (audio_format != 1 || info->num_channels != 1 || info->bits_per_sample != 16) {

return -1; // Only support mono, 16-bit PCM

}



// Find data chunk

offset += 8 + *(uint32_t *)(wav_data + offset + 4);

while (offset + 8 < wav_size) {

if (strncmp((char *)(wav_data + offset), "data", 4) == 0) {

info->data_size = *(uint32_t *)(wav_data + offset + 4);

info->data_start = wav_data + offset + 8;

return 0;

}

offset += 8 + *(uint32_t *)(wav_data + offset + 4);

}

return -1;

}

Filling audio as per below API


#define AUDIO_BUFFER_SIZE 4096

uint32_t wav_index = 0;



void fill_audio_buffer(void) {

uint32_t samples_to_copy = AUDIO_BUFFER_SIZE;

if (wav_index + samples_to_copy > wav_info.data_size / 2) {

samples_to_copy = (wav_info.data_size / 2) - wav_index;

}

memcpy(audio_buffer,

(int16_t *)(wav_info.data_start + wav_index * 2),

samples_to_copy * sizeof(int16_t));



wav_index += samples_to_copy;

}

Audio Play API

static int audio_play(uint16_t *paudioBuff, uint32_t len)

{

if(HAL_OK != HAL_SAI_Transmit_DMA(saiptr,(uint8_t*)paudioBuff, AUDIO_BUFFER_SIZE))

{

return -1;

}

return 0;

}

 

int wavPlayer_play(tas2110_data_t *tas_data)

{

uint32_t wav_size = _swav_data_end - _swav_data_start;

file_size = wav_size;

if (parse_wav_file(_wav_data, wav_size, &wav_info) != 0)

{

return -1;

}



tas2110_Configuration(tas_data);



fill_audio_buffer();

if(audio_play((uint16_t *)&audio_buffer[0], AUDIO_BUFFER_SIZE) != 0)

{

return -1;

}

return 0;

}

Callback APIs:

void HAL_SAI_TxHalfCpltCallback(SAI_HandleTypeDef *hsai)

{

fill_audio_buffer();

HAL_SAI_Transmit_DMA(hsai, (uint8_t*)audio_buffer, AUDIO_BUFFER_SIZE);

}



void HAL_SAI_TxCpltCallback(SAI_HandleTypeDef *hsai)

{

fill_audio_buffer();

HAL_SAI_Transmit_DMA(hsai, (uint8_t*)audio_buffer, AUDIO_BUFFER_SIZE);

}

 

    This topic has been closed for replies.
    Best answer by Saket_Om

    Hello @Jinal 

    Why did you set pNodeConfig.Init.DestInc to DMA_DINC_INCREMENTED ? In your case (DMA memory to peripheral), it should be set to DMA_DINC_FIXED.

    Please review the example I provided earlier for reference.

    3 replies

    Technical Moderator
    September 10, 2025
    JinalAuthor
    Visitor II
    September 11, 2025

    Hi @Saket_Om 

    Thanks for the response.

    I’m using the same example, but the DMA callback is not triggered in Linked-List mode.
    If I disable Linked-List and switch to List + Standard Request mode, I only get one buffer of output on the speaker (sounds like noise), and the callback is called only once.

    Attached are the .c and .ioc files for reference.
    Please advise if I’m missing something in the configuration.

    Thank you

    Jinal

    Technical Moderator
    September 11, 2025

    Hello @Jinal 

    You are not enabling the DMA interrupt in your code.

    please add the instruction below in MX_GPDMA1_Init()

     HAL_NVIC_EnableIRQ(GPDMA1_Channel12_IRQn);
    JinalAuthor
    Visitor II
    September 12, 2025

    Hi @Saket_Om 

    As mentioned earlier, when I configure the channel in Linked List mode instead of Standard Request mode, I do not receive any DMA callbacks.

    I have tried the same GPDMA configuration as suggested previously. For now, I am focusing only on the Linked List mode, but I am not getting any interrupts. Could you please advise how to resolve this issue?

    Below is my updated MX_GPDMA1_Init function:

    static void MX_GPDMA1_Init(void)
    {
    /* Peripheral clock enable */
    __HAL_RCC_GPDMA1_CLK_ENABLE();

    /* GPDMA1 interrupt Init */
    HAL_NVIC_SetPriority(GPDMA1_Channel12_IRQn, 0, 0);

    handle_GPDMA1_Channel12.Instance = GPDMA1_Channel12;
    handle_GPDMA1_Channel12.InitLinkedList.Priority = DMA_HIGH_PRIORITY;
    handle_GPDMA1_Channel12.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
    handle_GPDMA1_Channel12.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
    handle_GPDMA1_Channel12.InitLinkedList.TransferEventMode = DMA_TCEM_LAST_LL_ITEM_TRANSFER;
    handle_GPDMA1_Channel12.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;

    if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel12) != HAL_OK)
    {
    Error_Handler();
    }

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel12, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
    Error_Handler();
    }
    }

    Could you please guide me on why callbacks are not triggered in Linked List mode, and what additional configuration might be missing?

    Technical Moderator
    September 12, 2025

    Could you share your whole project please?

    JinalAuthor
    Visitor II
    September 15, 2025

    Sure, I’ve attached my project here.

     

    Saket_OmAnswer
    Technical Moderator
    September 15, 2025

    Hello @Jinal 

    Why did you set pNodeConfig.Init.DestInc to DMA_DINC_INCREMENTED ? In your case (DMA memory to peripheral), it should be set to DMA_DINC_FIXED.

    Please review the example I provided earlier for reference.