Skip to main content
Visitor II
January 4, 2026
Question

Understanding of HRTIM and DMA

  • January 4, 2026
  • 0 replies
  • 40 views

Hi all,

I am using the HRTIM unit of the STM32G474 to generate a PWM on channel A that depends on capture values of channel B. The channel B capture 1 value defines the channel A compare value and channel B capture 2 the channel A compare 2. The capture 1 event occurs during the first half of the switching period and capture 2 during the second half. 
Additional, the compare values need to be loaded with a default value if no capture event occurs.

I am using two interrupts to copy the data from the capture to the compare at the moment but I would like to use the DMA for this.

My idea was to use Peripheral to Peripheral transfer but I have only Memory to Peripheral and Peripheral to Memory in CubeMX. Is this a hardware limitation of the STM32G474 or is that a CubeMX limitation? Or is there a workaround by using a memory location?

My second problem is understanding of the DMA request. Can one timer channel generate more than one DMA request (one for each capture event) and connect that to 2 DMA channels? CubeMX allows only to connect 1 DMA channel per timer channel.

My understanding at the moment would require to use DMA request triggers from 6 HRTIM channels:
2 events to copy the capture values to memory
2 slightly delayed events (triggered by the capture events) to copy from memory to capture
2 events to copy the default values from memory to the capture registers (that is overwritten if the capture event is triggered).

The controller has the 6 timer channels, but I hope there is a better solution.

Kind Regards 
 Thundernail

 

    This topic has been closed for replies.