USB Audio on USB HS issue (cannot transmit data using ISO IN EP)
Hello,
I am having issue implementing USB Audio using the USB HS peripheral on STM32F767II.
Basically everything (enumeration, various control transfers (volume/mute), playback) works except recording. Specifically I am having trouble transmitting samples using the isochronous IN endpoint.
What I do:
- I call USBD_LL_Transmit to enqueue 96B of data to TX FIFO. MaxPacketSize is 96B. 1ms worth of samples (48kHz, mono, 16 bits).
- If ITTXFE happens - I disable the endpoint, flush the FIFO and call USBD_LL_Transmit with next batch of samples.
- If only IISOIXFR happens, host has not sent IN token. Interval in EP descriptor is set to 1ms, on HS one microframe is 1/8ms, so this will happen 7 out of 8 times. I just flip the EONUM bit in DIEPCTLx (using SODDFRM and SEVNFRM bits) to arm the EP for next microframe.
- Eventually I get XFRC (transfer completed) and I move on to next 96B of samples.
Everything looks ok (XFRC asserts each 1ms) but the host does not receive any data (looks like only zero-length-packets are coming). The PKTCNT and XFRSIZ in DIEPTSIZx are both zero when XFRC asserts. But what looks very weird to me - the DTXFSTSx immediately after the XFRC tells that only 5 words (20B) are available. The TX FIFO for this EP is set to 25 words (100B). After XFRC should it not be empty? I.e DTXFSTSx == 25?
Any ideas would be welcomed.