Skip to main content
Graduate
June 9, 2025
Question

USB CDC Communication between STM32 and PC

  • June 9, 2025
  • 2 replies
  • 836 views

Hello everyone,

I am currently working on a project using an STM32H755ZIT6 MCU and want to use the USB CDC class to send data over USB. I can successfully program the MCU and the system clock configuration is correct. However, when I plug in the USB, the device is not recognized by Windows. I receive the following error message:

  • "Unknown USB Device (Device Descriptor Request Failed)"

  • "The last USB device you connected to this computer malfunctioned, and Windows does not recognize it."

Schematic details:

_oepfel_1-1749456937816.png

I have attached the schematic of the USB circuit to this post.

  • USB_DP is connected to PA12.

  • USB_DN is connected to PA11.

  • The circuit is powered via USB as well.

  • Currently, only R45 and R50 are mounted (0 Ohm), R47 and R49 are not mounted.

  • The TS3USB30EDGSR chip is not activated at this stage. I have the option to activate it if needed.

To make sure the MCU has enough time after power-up, I added a 3-second delay before initializing the USB stack.

Still, the USB device is not recognized.

If anyone has an idea what could be wrong, or if you want to see more files (like code, initialization settings, etc.), feel free to let me know.

Thank you for your help!

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "usb_device.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

#include "usbd_cdc_if.h"
#include "string.h"
#include <stdbool.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

#ifndef HSEM_ID_0
#define HSEM_ID_0 (0U) /* HW semaphore 0*/
#endif

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
ADC_HandleTypeDef hadc2;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
static void MPU_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC1_Init(void);
static void MX_ADC2_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void writeData2Array(uint16_t measuredData, uint8_t *data_Array_CHx) {
	// first Byte
	// | half | CH1/2 | D5 | D4 | D3 | D2 | D1 | D0 |
	// seconde Byte
	// | half | CH1/2 | D11 | D10 | D9 | D8 | D7 | D6 |
	// Legende
	// half = 0 --> first Byte
	// half = 1 --> seconde Byte
	// CH1/2 = 0 --> CH1
	// CH1/2 = 1 --> CH2

	data_Array_CHx[0] = (data_Array_CHx[0] & 0b01000000)
			| (measuredData & 0b00111111);
	data_Array_CHx[1] = (data_Array_CHx[1] & 0b11000000)
			| ((measuredData >> 6) & 0b00111111);
}
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void) {

	/* USER CODE BEGIN 1 */

	/* USER CODE END 1 */
	/* USER CODE BEGIN Boot_Mode_Sequence_0 */
	int32_t timeout;
	/* USER CODE END Boot_Mode_Sequence_0 */

	/* MPU Configuration--------------------------------------------------------*/
	MPU_Config();

	/* USER CODE BEGIN Boot_Mode_Sequence_1 */
	/* Wait until CPU2 boots and enters in stop mode or timeout*/
// timeout = 0xFFFF;
// while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));
// if ( timeout < 0 )
// {
// Error_Handler();
// }
	/* USER CODE END Boot_Mode_Sequence_1 */
	/* MCU Configuration--------------------------------------------------------*/

	/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
	HAL_Init();

	/* USER CODE BEGIN Init */

	/* USER CODE END Init */

	/* Configure the system clock */
	SystemClock_Config();

	/* Configure the peripherals common clocks */
	PeriphCommonClock_Config();
	/* USER CODE BEGIN Boot_Mode_Sequence_2 */
	/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of
	 HSEM notification */
	/*HW semaphore Clock enable*/
	__HAL_RCC_HSEM_CLK_ENABLE();
	/*Take HSEM */
	HAL_HSEM_FastTake(HSEM_ID_0);
	/*Release HSEM in order to notify the CPU2(CM4)*/
	HAL_HSEM_Release(HSEM_ID_0, 0);
	/* wait until CPU2 wakes up from stop mode */
	timeout = 0xFFFF;
	while ((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0))
		;
	if (timeout < 0) {
		Error_Handler();
	}
	/* USER CODE END Boot_Mode_Sequence_2 */

	/* USER CODE BEGIN SysInit */
	HAL_Delay(3000);

	/* USER CODE END SysInit */

	/* Initialize all configured peripherals */
	MX_GPIO_Init();
	MX_ADC1_Init();
	MX_ADC2_Init();
	MX_USB_DEVICE_Init();
	/* USER CODE BEGIN 2 */

	/* USER CODE END 2 */

	/* Infinite loop */
	/* USER CODE BEGIN WHILE */

#define ADC_BUFFER_SIZE 1
	uint16_t ch1_adcValue[ADC_BUFFER_SIZE];

//	HAL_ADC_Start_DMA(&hadc1, (uint32_t*) ch1_adcValue, ADC_BUFFER_SIZE);

// first Byte
// | half | CH1/2 | D5 | D4 | D3 | D2 | D1 | D0 |
// seconde Byte
// | half | CH1/2 | D11 | D10 | D9 | D8 | D7 | D6 |
// Legende
// half = 0 --> first Byte
// half = 1 --> seconde Byte
// CH1/2 = 0 --> CH1
// CH1/2 = 1 --> CH2
	uint8_t data_Array_CH1[2];
	data_Array_CH1[0] = 0b00000000;
	data_Array_CH1[1] = 0b10000000;

	uint8_t data_Array_CH2[2];
	data_Array_CH2[0] = 0b01000000;
	data_Array_CH2[1] = 0b11000000;

//	uint16_t ch1_adcValue = 0;

	char str[64];
//	HAL_ADC_Start(&hadc1);
//	HAL_ADC_Start(&hadc2);
	while (1) {
		//		writeData2Array(0x7FF, data_Array_CH1);
		//		writeData2Array(0b101010101010, data_Array_CH2);
		//
		//		while (USBD_OK
		//				!= CDC_Transmit_FS(data_Array_CH1, sizeof(data_Array_CH1)))
		//		{
		//
		//		}
		//		while (USBD_OK
		//				!= CDC_Transmit_FS(data_Array_CH2, sizeof(data_Array_CH2)))
		//		{
		//
		//		}
		//

		//	 uint32_t combined = adc_buffer[0]; // ADC1 + ADC2 packed
		//
		//	 uint16_t adc_val1 = combined & 0xFFFF;
		//	 uint16_t adc_val2 = (combined >> 16) & 0xFFFF;

		//		writeData2Array(adc_val1, data_Array_CH1);
		//		writeData2Array(adc_val2, data_Array_CH2);
		//
		//		sprintf(str2, "CH1: %04u		CH2: %04u\n", adc_val1, adc_val2);
		//
		//		while (USBD_OK != CDC_Transmit_FS(str2, strlen(str2)))
		//		{
		//
		//		}

		HAL_ADC_Start(&hadc1);
		HAL_ADC_Start(&hadc2);

		HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);
		uint16_t adc_val1 = HAL_ADC_GetValue(&hadc1);

		HAL_ADC_PollForConversion(&hadc2, HAL_MAX_DELAY);
		uint16_t adc_val2 = HAL_ADC_GetValue(&hadc2);

		HAL_ADC_Stop(&hadc1);
		HAL_ADC_Stop(&hadc2);

		writeData2Array(adc_val1, data_Array_CH1);
		writeData2Array(adc_val2, data_Array_CH2);

//		sprintf(str, "CH1: %04u		CH2: %04u\n", adc_val1, adc_val2);

//		while (USBD_OK != CDC_Transmit_FS(str, strlen(str)))
//		{
//
//		}

		while (USBD_OK
				!= CDC_Transmit_FS(data_Array_CH1, strlen(data_Array_CH1))) {

		}

		while (USBD_OK
				!= CDC_Transmit_FS(data_Array_CH2, strlen(data_Array_CH2))) {

		}

		HAL_Delay(1);
		/* USER CODE END WHILE */

		/* USER CODE BEGIN 3 */
	}
	/* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void) {
	RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };
	RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0 };

	/** Supply configuration update enable
	 */
	HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

	/** Configure the main internal regulator output voltage
	 */
	__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

	while (!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {
	}

	/** Initializes the RCC Oscillators according to the specified parameters
	 * in the RCC_OscInitTypeDef structure.
	 */
	RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
	RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
	RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
	RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
	RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
	RCC_OscInitStruct.PLL.PLLM = 4;
	RCC_OscInitStruct.PLL.PLLN = 60;
	RCC_OscInitStruct.PLL.PLLP = 2;
	RCC_OscInitStruct.PLL.PLLQ = 2;
	RCC_OscInitStruct.PLL.PLLR = 2;
	RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
	RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
	RCC_OscInitStruct.PLL.PLLFRACN = 0;
	if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
		Error_Handler();
	}

	/** Initializes the CPU, AHB and APB buses clocks
	 */
	RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
			| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_D3PCLK1
			| RCC_CLOCKTYPE_D1PCLK1;
	RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
	RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
	RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
	RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
	RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
	RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
	RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

	if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK) {
		Error_Handler();
	}
}

/**
 * @brief Peripherals Common Clock Configuration
 * @retval None
 */
void PeriphCommonClock_Config(void) {
	RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = { 0 };

	/** Initializes the peripherals clock
	 */
	PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC;
	PeriphClkInitStruct.PLL2.PLL2M = 32;
	PeriphClkInitStruct.PLL2.PLL2N = 129;
	PeriphClkInitStruct.PLL2.PLL2P = 2;
	PeriphClkInitStruct.PLL2.PLL2Q = 2;
	PeriphClkInitStruct.PLL2.PLL2R = 2;
	PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_1;
	PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
	PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
	PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
	if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) {
		Error_Handler();
	}
}

/**
 * @brief ADC1 Initialization Function
 * None
 * @retval None
 */
static void MX_ADC1_Init(void) {

	/* USER CODE BEGIN ADC1_Init 0 */

	/* USER CODE END ADC1_Init 0 */

	ADC_MultiModeTypeDef multimode = { 0 };
	ADC_ChannelConfTypeDef sConfig = { 0 };

	/* USER CODE BEGIN ADC1_Init 1 */

	/* USER CODE END ADC1_Init 1 */

	/** Common config
	 */
	hadc1.Instance = ADC1;
	hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
	hadc1.Init.Resolution = ADC_RESOLUTION_12B;
	hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
	hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
	hadc1.Init.LowPowerAutoWait = DISABLE;
	hadc1.Init.ContinuousConvMode = ENABLE;
	hadc1.Init.NbrOfConversion = 1;
	hadc1.Init.DiscontinuousConvMode = DISABLE;
	hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
	hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
	hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
	hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
	hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
	hadc1.Init.OversamplingMode = DISABLE;
	hadc1.Init.Oversampling.Ratio = 1;
	if (HAL_ADC_Init(&hadc1) != HAL_OK) {
		Error_Handler();
	}

	/** Configure the ADC multi-mode
	 */
	multimode.Mode = ADC_MODE_INDEPENDENT;
	if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK) {
		Error_Handler();
	}

	/** Configure Regular Channel
	 */
	sConfig.Channel = ADC_CHANNEL_2;
	sConfig.Rank = ADC_REGULAR_RANK_1;
	sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
	sConfig.SingleDiff = ADC_SINGLE_ENDED;
	sConfig.OffsetNumber = ADC_OFFSET_NONE;
	sConfig.Offset = 0;
	sConfig.OffsetSignedSaturation = DISABLE;
	if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
		Error_Handler();
	}
	/* USER CODE BEGIN ADC1_Init 2 */

	/* USER CODE END ADC1_Init 2 */

}

/**
 * @brief ADC2 Initialization Function
 * None
 * @retval None
 */
static void MX_ADC2_Init(void) {

	/* USER CODE BEGIN ADC2_Init 0 */

	/* USER CODE END ADC2_Init 0 */

	ADC_ChannelConfTypeDef sConfig = { 0 };

	/* USER CODE BEGIN ADC2_Init 1 */

	/* USER CODE END ADC2_Init 1 */

	/** Common config
	 */
	hadc2.Instance = ADC2;
	hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
	hadc2.Init.Resolution = ADC_RESOLUTION_12B;
	hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
	hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
	hadc2.Init.LowPowerAutoWait = DISABLE;
	hadc2.Init.ContinuousConvMode = ENABLE;
	hadc2.Init.NbrOfConversion = 1;
	hadc2.Init.DiscontinuousConvMode = DISABLE;
	hadc2.Init.ExternalTrigConv = ADC_SOFTWARE_START;
	hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
	hadc2.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
	hadc2.Init.Overrun = ADC_OVR_DATA_PRESERVED;
	hadc2.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
	hadc2.Init.OversamplingMode = DISABLE;
	hadc2.Init.Oversampling.Ratio = 1;
	if (HAL_ADC_Init(&hadc2) != HAL_OK) {
		Error_Handler();
	}

	/** Configure Regular Channel
	 */
	sConfig.Channel = ADC_CHANNEL_5;
	sConfig.Rank = ADC_REGULAR_RANK_1;
	sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
	sConfig.SingleDiff = ADC_SINGLE_ENDED;
	sConfig.OffsetNumber = ADC_OFFSET_NONE;
	sConfig.Offset = 0;
	sConfig.OffsetSignedSaturation = DISABLE;
	if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK) {
		Error_Handler();
	}
	/* USER CODE BEGIN ADC2_Init 2 */

	/* USER CODE END ADC2_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void) {
	/* USER CODE BEGIN MX_GPIO_Init_1 */

	/* USER CODE END MX_GPIO_Init_1 */

	/* GPIO Ports Clock Enable */
	__HAL_RCC_GPIOB_CLK_ENABLE();
	__HAL_RCC_GPIOF_CLK_ENABLE();
	__HAL_RCC_GPIOA_CLK_ENABLE();

	/* USER CODE BEGIN MX_GPIO_Init_2 */

	/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/* MPU Configuration */

void MPU_Config(void) {
	MPU_Region_InitTypeDef MPU_InitStruct = { 0 };

	/* Disables the MPU */
	HAL_MPU_Disable();

	/** Initializes and configures the Region and the memory to be protected
	 */
	MPU_InitStruct.Enable = MPU_REGION_ENABLE;
	MPU_InitStruct.Number = MPU_REGION_NUMBER0;
	MPU_InitStruct.BaseAddress = 0x0;
	MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
	MPU_InitStruct.SubRegionDisable = 0x87;
	MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
	MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
	MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
	MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
	MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
	MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

	HAL_MPU_ConfigRegion(&MPU_InitStruct);
	/* Enables the MPU */
	HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void) {
	/* USER CODE BEGIN Error_Handler_Debug */
	/* User can add his own implementation to report the HAL error return state */
	__disable_irq();
	while (1) {
	}
	/* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

    This topic has been closed for replies.

    2 replies

    ST Employee
    June 9, 2025

    Hello @_oepfel  , 

    Please try using the provided a CDC example on the STM32H747I-EVAL board. You can port it to your specific board.

    NB : Follow the instructions in the README file, which includes all the necessary steps to ensure your project works correctly.

    In fact  This is a typical application on how to use the STM32H747xx USB OTG Device peripheral where the STM32 MCU behaves as a USB-to-RS232 bridge following the Virtual COM Port (VCP) implementation. -

    - On one side, the STM32 exchanges data with a PC host through USB interface in Device mode.

    - On the other side, the STM32 exchanges data with other devices (same host, other host, other devices…) through the UART interface (RS232).

    Regarding your issue where the USB device is not recognized, this could potentially be a hardware-related problem. Please try the following troubleshooting steps:

    Try plugging the device into a different USB port,  & Replace the USB cable: Sometimes the USB cable may be damaged, replace the cable with a new one to see if that solves the problem.

    Br

     

    Technical Moderator
    June 9, 2025

    Hi @_oepfel 

     

    In addition to the points mentioned by @MOBEJ . 

    • Verify that the USB_DP and USB_D are routed as a differential pair with 90 Ω ± 10% impedance.
    • Minimize stubs and ensure the ESD protection device does not introduce significant impedance discontinuities

    You can refer to this schematics as starting point.