USB connection between STM32F411 and modem RM500 quectel
Hi I am working on a project where a need to send AT commands through my MCU to a modem, the problem is that this modem only has a USB interface and not a UART interface, so I have a lot of doubts of how should I do this, i wanted to use the USB_Host_Library but I dont know hot to send the data to a certain interface and enpoint, since que AT command interface appears as a virtual COM (Interface 2 with 3 endpoints).
And which class should I use? Communication Host class?
Thanks in advice, Nicolas.