USB Dual VCOM Composite Device
Hi,
I managed to implement a dual VCOM composite device for an STM32H7. In principal the communication works, if both COM ports are actively used/open. One port is used for sending commands and receiving responses. The other one sends out unsolicited trace data and can be opened/closed arbitrarily.
The problem arises once I close the trace VCOM. It seems like after calling
uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)
{
uint8_t result = USBD_OK;
/* USER CODE BEGIN 7 */
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
if (hcdc->TxState != 0){
return USBD_BUSY;
}
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, Buf, Len);
result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);
/* USER CODE END 7 */
return result;
}hcdc->TxState stays true, which also stalls the communication on the other port. The code here was copied from a code example for an STM32H7 eval board, I think.
Only when the trace port is re-opened (in a generic terminal application)
static uint8_t USBD_CDC_DataIn(USBD_HandleTypeDef *pdev, uint8_t epnum)is called again, which resets this state.
I see that there is the possibility to detect the start of the session with
static int8_t CDC_Control_FS(uint8_t cmd, uint8_t* pbuf, uint16_t length)where LINE CODING Request/Responses and CONTROL LINE STATE requests are exchanged.
However when a port is closed, the USB host just sends the exact same CONTROL LINE STATE to the device as when opening it (tested on multiple terminal applications). Is there any way to safely detect the closing? Or implement a timeout mechanism the remove the "lock" again?
Thanks in advance for your help.