USB FS not sending correct amount of data
Hello
I have been trying to debug an USB issue I've had on my STM32F722 Nucleo. For whatever input I try to send with CDC only two bytes are sent to my host PC. I'm using the latest HAL drivers.
When breaking in the function USB_WritePacket() I can see that the contents of DIEPTSIZ3 are as exptected (MCNT = 0, PTKCNT = 1, XFRSIZ = 26) and the contents of pSrc are correct. When I step through the loop I can see that DTXFSTS3 is decreasing by one for each write to the FIFO. Once all 7 32 bit words are written I can see activity on my host PC.
So far everything works as expected.
But when I check on my PC with Wireshark (And COM teminal) I only receive two bytes. The value of these bytes seems random, but stays the same until I recompile.
Thanks in advance for any help solving this
/Jacob