USB high speed fails to enumarate
Hi All!
I'm trying to use USB high speed in STM32h723 with an external phy usb3300.
I started the program from the CubeMx Ux_Device_CDC_ACM which uses the internal phy.
I modified the clocks and the USB module to use an external phy USB3300 and so far it works fine in Full Speed.
My problem is that when I try to use it at High Speed, the enumeration is not going well and the device is not recognised by the PC (win10).
With a USB protocol analyser, I got this when High speed is set: Got stuck in with device configuration
Chirp, passation of data with address setting and device descriptor seems to work

And This is Full Speed: Works fine

With an oscilloscope, I check the 60M clock, and the timing of DIR, NEXT, and STP signals relative to the CLK.
Even though they are not very clean signals there are within the data sheet limitations.
My questions:
1. Anyone with the idea of what I Should do?
2. Where in the program can I look to debug the functions handling the enumeration of the USB?
I have USBX, ThreadX in the project and I francky don't know who is handling who?
I feel that if I can just put a wait after each descriptor or force the program to send each descriptor 3times,
I might pass that stage and get the device recognised by the PC.
Thanks in advance.