USB-Host CDC STM32F4, why are 2 USB_CDC_ReceiveCallback interrupts called when 64bytes are received ?
I want to programme a USB host CDC. This works as far as it goes.
This means I can receive and send data.
My problem is that the receive interrupt is called 2 times for data packets with 64 bytes.
It is also always called once too often for packets >64 bytes. This means that it is called 3 times for 128 bytes.
The result is that I always receive the last packet 2 times.
Has anyone already observed this problem?
Best regards
Snumeli