USB HS on the STM32H7S3L8
Hello,
I'm trying to use the USB-HS peripheral with the built-in PHY on Nucleo STM32H7S3L8
I'm using CubeMX generated code from CubeIDE. I have not chosen the Nucleo board on CubeMX, because it was causing some issues with the MPU. Instead, I've chosen the MCU (STM32H7S3L8).
The peripheral times out during initialization at a usb core soft reset, just after enabling the internal PHY. What am I doing wrong? Has anyone been able to use the USB HS PHY on this device/board.
This is the USB_CoreReset call where I am getting a HAL_TIMEOUT:
HAL_StatusTypeDef USB_CoreInit(USB_OTG_GlobalTypeDef *USBx, USB_OTG_CfgTypeDef cfg)
{
HAL_StatusTypeDef ret;
#if defined (USB_OTG_HS)
if (USBx == USB_OTG_HS)
{
if (cfg.phy_itface == USB_OTG_HS_EMBEDDED_PHY)
{
/* Init The UTMI Interface */
USBx->GUSBCFG &= ~(USB_OTG_GUSBCFG_TSDPS);
}
/* Reset after a PHY select */
ret = USB_CoreReset(USBx);
...
These are the things in the code which are possibly relevant :

RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USBPHYC;
PeriphClkInit.UsbPhycClockSelection = RCC_USBPHYCCLKSOURCE_HSE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) { die(); }
__HAL_RCC_USBPHYC_CLK_ENABLE();
__HAL_RCC_USB_OTG_HS_CLK_ENABLE();
HAL_NVIC_SetPriority(USB_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USB_IRQn);
if(HAL_PWREx_EnableUSBVoltageDetector() != HAL_OK) { die(); }
usb_hpcd.Instance = USB_OTG_HS;
usb_hpcd.Init.speed = PCD_SPEED_HIGH;
usb_hpcd.Init.dev_endpoints = CFG_TUD_ENDPOINTS;
usb_hpcd.Init.dma_enable = DISABLE;
usb_hpcd.Init.phy_itface = USB_OTG_HS_EMBEDDED_PHY;
usb_hpcd.Init.Sof_enable = DISABLE;
usb_hpcd.Init.low_power_enable = DISABLE;
usb_hpcd.Init.lpm_enable = ENABLE;
usb_hpcd.Init.vbus_sensing_enable = DISABLE;
usb_hpcd.Init.use_dedicated_ep1 = DISABLE;
usb_hpcd.Init.vbus_sensing_enable = DISABLE;
HAL_StatusTypeDef result = HAL_PCD_Init(&usb_hpcd);
if (result != HAL_OK){
die();
};
This is the main clock configuration :
void clock_set_default(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE0) != HAL_OK)
{
die();
}
/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSE
|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL1.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL1.PLLM = 2;
RCC_OscInitStruct.PLL1.PLLN = 50;
RCC_OscInitStruct.PLL1.PLLP = 1;
RCC_OscInitStruct.PLL1.PLLQ = 2;
RCC_OscInitStruct.PLL1.PLLR = 2;
RCC_OscInitStruct.PLL1.PLLS = 2;
RCC_OscInitStruct.PLL1.PLLT = 2;
RCC_OscInitStruct.PLL1.PLLFractional = 0;
RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL2.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL2.PLLM = 3;
RCC_OscInitStruct.PLL2.PLLN = 50;
RCC_OscInitStruct.PLL2.PLLP = 2;
RCC_OscInitStruct.PLL2.PLLQ = 4;
RCC_OscInitStruct.PLL2.PLLR = 2;
RCC_OscInitStruct.PLL2.PLLS = 2;
RCC_OscInitStruct.PLL2.PLLT = 1;
RCC_OscInitStruct.PLL2.PLLFractional = 0;
RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL3.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL3.PLLM = 3;
RCC_OscInitStruct.PLL3.PLLN = 50;
RCC_OscInitStruct.PLL3.PLLP = 2;
RCC_OscInitStruct.PLL3.PLLQ = 4;
RCC_OscInitStruct.PLL3.PLLR = 4;
RCC_OscInitStruct.PLL3.PLLS = 8;
RCC_OscInitStruct.PLL3.PLLT = 2;
RCC_OscInitStruct.PLL3.PLLFractional = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
die();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK4|RCC_CLOCKTYPE_PCLK5;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
RCC_ClkInitStruct.APB5CLKDivider = RCC_APB5_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{
die();
}
}
The HSE on the board is 24MHz, though I don't think there is any place in the code where this is defined for the USB PLL to be correctly configured. I also don't seem to have done anything to enable the USB PHY other than too enable the PHYC clock.
I have also not done anything with the UCPD, though the nucleo is wired to a Type C port with another IC involved for USB C PD control. Could this cause the PHY to not startup?
Any suggestions would be appreciated.