USB PD Dead Battery pin usage when functioning as PD Source
I am using the STM32G071GBU6N to implement 2 USB PD interfaces. Port 1 will be sink, Port 2 will be source. On the sink interface, the dead battery support is needed and DBCC pins will be connected to cc pins. On the source, I do not need dead battery support. I want to reuse the DBCC pins for other use. The ref manual indicates that they should be connected to ground. Is this necessary, or can they be reused when operating as source only?