Question
USB read failing in standard 32H743 USB MSC with 16GB pen drive
A BOT protocol read fail error is occurring in usbh_msc.bot.c:- See "*** MY MOD-" below
USBH_StatusTypeDef USBH_MSC_BOT_Process (USBH_HandleTypeDef *phost, uint8_t lun)
{
...
else if (URB_Status == USBH_URB_STALL)
{
/* This is Data IN Stage STALL Condition */
MSC_Handle->hbot.state = BOT_ERROR_IN;
/* Refer to USB Mass-Storage Class : BOT (www.usb.org)
6.7.2 Host expects to receive data from the device
3. On a STALL condition receiving data, then:
The host shall accept the data received.
The host shall clear the Bulk-In pipe.
4. The host shall attempt to receive a CSW.*/
#if (USBH_USE_OS == 1)
osMessagePut ( phost->os_event, USBH_URB_EVENT, 0);
#endif
}
else if (URB_Status == USBH_URB_ERROR) // *** MY MOD- *** added as getting error here!
{
/* This is Data IN Stage ERROR Condition */
MSC_Handle->hbot.state = BOT_ERROR_IN; // tried this but no change
}
break;
case BOT_DATA_OUT:
...