USB SOF period incorrect in host mode during CSleep on STM32H743
My OTG_HS2 kernel clock is PLL3Q at 48 MHz. If I use CSleep (only CSleep, not any of the deep sleep modes), SOFs are generated at the wrong interval (checked with protocol analyzer and oscilloscope). If I remove the WFI, SOFs are generated at the proper interval. It seems that either CSleep is gating the USB clock or else it is turning off PLL3, neither of which it should do. Has anyone else seen this?