uSD not work in Riverdi 121STM32H7_1_6
Hello everybody.
I bought Riverdi STM32 Embedded Display RVT121HVSNWC00-B
I create my first project using touch GFX.
I generate code and import it in STM32CubeIDE.
I format FAT32 a 128G uSD using custom program.
I plug the uSD into adapter and I write this code.

fresult is FS_NOT_READY and I don't understand the reason.
Here my configuration.











I notice in the main that there is FATFS initialization

but I don't find a call to MX_SDMMC1_SD_Init.
If I force this call after FATFS initlization the code run in ErrorHandler, but if I inpect hsd1.SdCard struct I see that card property are read correctly (I believe).

BlockSize x BlockNbr = 128G !! OK
Can someone help me ?
Thanks in advice