Use of .c or .h files
Hi, I am curious one thing when using the HAL libraries. Just as an basic exapmle i assign LED1 to PB12 pin of STM32F070CBT6 as an GPIO_output. And i want to use HAL_GPIO_WritePin(GPIOB, LED1, LED1_SET); instead of HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET); . Do you think it is weird that i want to use my variables like that with HAL libraries? Second thing is (if it is not weir or inappropriate), should i define my definitions as "definitions.c" or "definitions.h"? When i make some search, .c file is not recommended. I am not sure if i do all these steps with my ST microcontroller and it works well.