Question
Using a Nucleo-h723 and would like to, via USB DFU, load my program using the built-in bootloader.
Connections:
D- = PA11
D+ = PA12
and Gnd to Gnd
As well, Boot0 is connected to VDD. I have nothing connected to the UARTS or CAN.
Even with this setup, upon reset, the system runs the code I have downloaded (via ST-Link) rather than the bootloader. I think it may have something to do with the crystall.