Using bootloader GO command with BOOT0 always asserted
I am using the I2C bootloader on STM32L431, in a system where another host CPU exists. I would like to minimize the number of host GPIO needed to manage entry to bootloader mode. (Currently the host is controlling the BOOT0 and RST# pins). I would like to keep BOOT0 always asserted so STM32 boots into bootloader every time. The host would them command a jump to the application using the GO command.
With BOOT0 asserted, I find that the STM32 always jumps back into bootloader after issuing GO 0x08000000. Is that expected? I would have expected the BOOT0 check to be done by the bootloader code only at POR. I would expect that using the GO command to jump directly to the application reset vector 0x08000004 would bypass this checking of the state of the BOOT0 pin. Is there some way to accomplish this?
Thanks.