Question
Using both of the STM32H7 USB controllers as Host ports - issues?
Are there any issue using both controllers in host mode?
USBH_StatusTypeDef USBH_LL_Init(USBH_HandleTypeDef *phost)
{
/* Init USB_IP */
if (phost->id == HOST_FS)
{
/* Link the driver to the stack. */
hhcd_USB_OTG_FS.pData = phost;
phost->pData = &hhcd_USB_OTG_FS;
hhcd_USB_OTG_FS.Instance = USB_OTG_FS;
hhcd_USB_OTG_FS.Init.Host_channels = 16;
hhcd_USB_OTG_FS.Init.speed = HCD_SPEED_FULL;
hhcd_USB_OTG_FS.Init.dma_enable = DISABLE;
hhcd_USB_OTG_FS.Init.phy_itface = HCD_PHY_EMBEDDED;
hhcd_USB_OTG_FS.Init.Sof_enable = DISABLE; // GW8RDI NOTE todo try with SOF
if (HAL_HCD_Init(&hhcd_USB_OTG_FS) != HAL_OK)
{
Error_Handler( );
}
USBH_LL_SetTimer(phost, HAL_HCD_GetCurrentFrame(&hhcd_USB_OTG_FS));
}
return USBH_OK;
}