Using HAL NAND
Good afternoon.
I am configuring a NAND memory using FMC on the STM32H7. I am dealing with the following scenario: HCLK = 80 MHz (to match the example in AN4761) and a NAND memory SkyHigh Memory S34ML01G1 Following all the calculations specified in AN4761, I am encountering an error where the last byte fails on some pages. When a read is performed more than once, the byte is corrected, but there is this inconsistency. Where could the error be?