Using repetition count with PWM generates wrong number of events on STM32U5
Hello,
I am trying to use a timer 15 in PWM mode to drive the DMA of a DAC. I need the PWM to generate N number of update events for M number of pulses. For example, generated an update event 10 times every 200 pulses. I'm just trying to get the PWM working before checking if the DAC is working.
The problem I'm having is generating the correct number of update events from the PWM. At the moment, I'm not trying to count the number of update event's since it's not working. I am setting the repetition counter to 10; however, I only get like 4(or 3) update events and then 20ms of none. So for the events I do get, they are the correct number of pulse but I'm expecting to see the updates events running all the time, not blocks of 3-4.
I'm using Cube for configuring the timer but I do some manual config so I can change things in the code instead of depending on the config generated by Cube.
So in the timer init code I do the following in the user code section
uint32_t ps = HAL_RCC_GetPCLK2Freq()/1000000;
__HAL_TIM_SET_PRESCALER(&htim15, ps - 1);
__HAL_TIM_SET_AUTORELOAD(&htim15, (HAL_RCC_GetPCLK2Freq()/(ps * 10000)) - 1);
// enable interrupt, need so can count N update events
HAL_TIM_PWM_MspInit(&htim15);
Then in my default FreeRTOS task I do this. Note that the PWM does not enable the update event(which I need to drive DAC DMA) so I have to enable that manually.
LL_TIM_SetRepetitionCounter(htim15.Instance, (sizeof(vdef)/sizeof(vdef[0])-1));
// 50% for now
__HAL_TIM_SET_COMPARE(&htim15, TIM_CHANNEL_1, __HAL_TIM_GET_AUTORELOAD(&htim15)/2);
//HAL_DAC_Start_DMA(&hdac1, DAC_CHANNEL_1, vdef, sizeof(vdef)/sizeof(vdef[0]), DAC_ALIGN_12B_R);
// PWM does not enable update event
__HAL_TIM_ENABLE_IT(&htim15, TIM_IT_UPDATE);
// don't use Start_IT, we don't need CC events
HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_1);
However, as I said above, I'll get 3-4 update events and then nothing for 20ms, then get another 3-4 update events. However, I just discovered this morning that if I change the PWM to generate at 1kHz instead of 10kHz the update events are generated continuously.
The PWM output looks fine for both 1kHz and 10kHz and I don't understand what is causing the issue with the update event when I change the period?
thanks
Jeff