Using STM32 examples on custom boards
Hello,
I have made a custom board using the STM32WB55CEU6 chip and I would like to try out some examples that are available from ST. My problem is that these examples are made for STM32WB55CG and I can't find an easy way to change target of these examples. In the read me file it says:
This example has been tested with NUCLEO-G431KB RevA board and can be
easily tailored to any other supported device and development board.
But i can't seem to find an easy way to do it.
My current aproach is:
- Getting the example project using CubeMX.
- Creating new project with the desired target
- Importing .ioc project configuration
After that I have the same configuration but the project is obviously empty. The example files are linked so i can't copy them.
Thank you in advance for any help.