Question
Using STM32G4 with Zephyr and USB Networking
I am trying to stand up a project using an STM32G4 using Zephyr with USB Device Next Networking. I have a similar project up and running on an nRF52. I'm getting the error on my STM32 project that upon system reset, I get a hard fault in z_cstart() -> ... -> statics_init() -> sys_heap_init(). I've isolated this to be a problem when I turn on CONFIG_NET_L2_ETHERNET=y. If I set CONFIG_DEBUG=y I see a similar failure upon the call to z_bss_zero().
From what I can tell, the errors are consistent with an error initializing the soc memory. This is a custom board with a G473CC soc. I've made a custom zephyr dts for this board with #include <st/g4/stm32g473Xc.dtsi> so afaik the memory definitions should be correct.
I haven't set any memory protections in the option bytes, is there perhaps a default protection in place that comes from the factory that may be causing an issue?