Skip to main content
Visitor II
January 10, 2020
Solved

Using USB hub with STM32F7 USB HS

  • January 10, 2020
  • 6 replies
  • 2048 views

Hello,

I'm designing an embedded system that connects to a PC for USB data and converts it to an analog signal.

This is an HS USB device with 2 USB ports which needs to process 4 channel 40Mbps data.

This device can work as a single system, but with some setup, I want to make the device send 2 channels of the data to the same device system connected through another USB port.

Even though there are 2 USB peripherals in STM32F7 series, only 1 is HS and the other is FS. So I can't use FS port due to slow speed.

Also, I can't connect 1 computer to 2 systems directly due to some limitation.

Can the system diagram below achievable?

I couldn't think of a better way to implement this idea.

Thanks in advance.

0690X00000BvotTQAR.png

    This topic has been closed for replies.
    Best answer by T J

    I was suggesting that you take Usart1 over the the other processor.

    getting your system to recognize the USBHUB is not trivial.

    You'd probably shoe this in with a STM32MP1 , but not a STM32H or STM32F series processor.

    6 replies

    Visitor II
    January 10, 2020

    can you add extra DAC ports to the first system ?

    BHan.1Author
    Visitor II
    January 10, 2020

    Unfortunately no.

    Maybe because this is an application specific DAC, there's only one data port available.

    Visitor II
    January 10, 2020

    which dac is it ?

    BHan.1Author
    Visitor II
    January 10, 2020

    It's an high resolution audio DAC. So, basically I want to split Left and Right Channel to System 1 and 2.

    Visitor II
    January 10, 2020

    Let me see the DAC, see what we can do with two of them on one micro

    BHan.1Author
    Visitor II
    January 10, 2020

    It's a DAC by Cirrus Logic WM8740.

    And your suggestion of running 2 of them on one micro is very logical, but my actual goal is to have 2 separate system and link them by USB.

    Visitor II
    January 10, 2020

    ok,

    its only 192KHz throughput

    so you could redirect your stream to a serial port for the other board.

    230400 baud seems to work well, that's just enough for your bandwidth.

    you could go higher baud, using a "serial TTL" interface.

    BHan.1Author
    Visitor II
    January 10, 2020

    Is the below diagram what your are suggesting?

    I think this is a good option. I will be using USB C port so pin number is not a problem.

    If I not understanding you please let me know. Maybe you are saying data can be transferred using DP/DM pin without using MUX.

    0690X00000BvowhQAB.png

    T JAnswer
    Visitor II
    January 10, 2020

    I was suggesting that you take Usart1 over the the other processor.

    getting your system to recognize the USBHUB is not trivial.

    You'd probably shoe this in with a STM32MP1 , but not a STM32H or STM32F series processor.

    BHan.1Author
    Visitor II
    January 11, 2020

    Thanks for the suggestion.

    From your suggestion, I was thinking of compressing the audio little to make one channel under 12Mbps and use FS USB ports in STM32.

    USB Hub does seems to be a complicated matter.

    I will also check the STM32MP1 for the main MCU.

    Visitor II
    January 11, 2020
    BHan.1Author
    Visitor II
    January 14, 2020

    Thanks T J,

    I will check this out.