Skip to main content
Visitor II
November 29, 2019
Question

Using X-Cube-Azure IoT kit P-L96G-CELL01 with UG96 Cellular Modem. The push button switch is not recognized so I cannot enter cellular credentials or TLS root CA certificate. Using software version 1.2.0. Tried pressing blue (joystick) during …...

  • November 29, 2019
  • 1 reply
  • 599 views

Tera Term log:

Starting Main Thread...

*************************************************************

***  HWJ AZURE

***  STM32 IoT Discovery kit for

***     STM32F413/STM32F769/STM32L475/STM32L496 MCU

***  X-CUBE-AZURE Cloud Connectivity Demonstration

***  FW version: 1.2.0 - 17-July-2019 04:18:03 PM

*************************************************************

*** Board personalization ***

- Network Interface initialized:

- Network Interface starting:

*** C2C connection ***

Initializing the cellular module

- Network Interface connecting:

Start of network initialization

Trying to connect with the external SIM

Waiting for UG96 modem running

Signal not known or not detectable yet (be patient)

.............Module initialized successfully: Quectel

ProductID: UG96

FW version: UG96LNAR02A06E1G

SIM Id (IccID): 8944502802190659949F

- Network Interface started:

  - Device Name : Quectel.

  - Device ID : UG96.

  - Device Version : UG96LNAR02A06E1G.

..........

C2C module registered

Registration done in 20028 msseconds

Retrieving the cellular operator: "T-Mobile"

    This topic has been closed for replies.

    1 reply

    ST Employee
    January 17, 2020

    Hi,

    There's an issue in X-Cube-Azure 1.2.0 about this. It should be fixed in version 1.2.1 currently available on st.com.