Skip to main content
Explorer
January 22, 2024
Question

[version-going-backwards] error occurs when running bitbake.

  • January 22, 2024
  • 1 reply
  • 1310 views

 

When I add a debug log to the source code, a [version-going-backwards] error occurs.

ERROR: weston-cube-4.0+gitAUTOINC+cd44839e95-r0 do_packagedata_setscene: QA Issue: Package version for package weston-cube went backwards which would break package feeds (from 0:4.0+git0+cd44839e95-r0.1 to 0:4.0+git0+cd44839e95-r0.0) [version-going-backwards]

 

What should I do so that an error does not occur even if I add a debug log?

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    April 22, 2024

    Hi @kiichi ,

    I assume that this question remains without answer because there is not enough details.

    If you still facing an issue, could you please provide more details about used firmware and compiler also the steps you followed.

    If you have already identified the solution, please share it with our Community. That would be helpful for others.

    -Amel