Waking from STOP mode U575
I am trying to get the STM32U575 to wake from STOP3 mode using the NUCLEO-U575ZI-Q dev board. I followed the example to enable the wakeup pin, clear any pending wakeup flag, and then go to sleep. I have this configured to pin PC13 which is the user push button, but the button does not wake the mcu. The push button does work for waking from SLEEP mode using the interrupt from the same pin. Here is the code I used from the example:
/* Enable WakeUp Pin PWR_WAKEUP_PIN2 connected to PC.13 */
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2_HIGH_1);
HAL_NVIC_SetPriority(PWR_S3WU_IRQn, 0, 0);
NVIC_EnableIRQ(PWR_S3WU_IRQn);
HAL_SuspendTick();
/* Clear all related wakeup flags*/
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG2);
HAL_PWREx_EnterSTOP3Mode(PWR_SLEEPENTRY_WFI);
/* wake with push button*/
SystemClock_Config();
HAL_ResumeTick();
I'm using FreeRTOS but this code happens before FreeRTOS is initialized (for testing).
Any ideas why this is not working?