What are GPIO events? How do I connect an event to a peripheral, specifically the DMA?
I've been reading about GPIO and what can be triggered. I see an event can be triggered. Events can be connected to peripherals to have some control without the CPU intervening. I can't find good documentation showing how to connect or effect peripherals. I'm hoping there is a way to trigger a DMA channel to transfer data with a GPIO without a timer in between.
Are GPIO events the way to trigger a DMA transfer with an external signal? Interrupts are too slow. Timers can do it but are they necessary?