What is the difference in the implementation of Low power Sleep vs Sleep in STM32L053 using cubeIDE and HAL.
I went through the examples on the ST site which have the direct implementations (not using CubeIDE generated code HAL for GPIO, SystemClock, ... config implementation)
- https://github.com/STMicroelectronics/STM32CubeL0/blob/master/Projects/NUCLEO-L053R8/Examples/PWR/PWR_SLEEP/Src/main.c
- https://github.com/STMicroelectronics/STM32CubeL0/blob/master/Projects/NUCLEO-L053R8/Examples/PWR/PWR_LPSLEEP/Src/main.c
The only difference is that low power sleep requires to disable the prefetch buffer initially
__HAL_FLASH_PREFETCH_BUFFER_DISABLE(); /* Disable Prefetch Buffer */
and then before going into sleep mode, enable the powerdown during sleep
__HAL_FLASH_SLEEP_POWERDOWN_ENABLE();/* Enable the power down mode during Sleep mode */
are these the only differences? Do I need to disable the __HAL_FLASH_SLEEP_POWERDOWN after i wake the mcu up (there is no function for it and the definition of __HAL_FLASH_SLEEP_POWERDOWN_ENABLE seems sleep mode specific so it seems unlikely that I need to manually disable it)
Are the power consumption differences significant enough if I'm using a UART that's always listening?