What on earth the 'BootRAM' in startup file is?
I'm working on my cpp scaffold for stm32, so I read the startup file generated by STM32CubeMX.And I noticed that the startup file contains a definition called BootRAM, but there is no documentation on it.It also seems not being used anywhere else on a regular project, so what on earth it is?Should I consider it when I write my own startup file?
P.S. The startup code I've mentioned is below:
/* start address for the initialization values of the .data section.
defined in linker script */
.word _sidata
/* start address for the .data section. defined in linker script */
.word _sdata
/* end address for the .data section. defined in linker script */
.word _edata
/* start address for the .bss section. defined in linker script */
.word _sbss
/* end address for the .bss section. defined in linker script */
.word _ebss
.equ BootRAM, 0xF1E0F85F