What's the correct way to write THUMB/ARM instructions mixed with LL Drivers for the STM32F334?
I'm writting a very time-critical application for the STM32F334, where I have to control 4 power converters (mostly 3, one is time-shared another power converter). And recently I saw some ways to optimize code, like this:
//*********** 1360ns ****************
LL_HRTIM_TIM_SetCompare3(HRTIM1, LL_HRTIM_TIMER_A, DEF_TMRA_STATIC_MAX_PWM_CTE+i_CalcDutyA);
LL_HRTIM_TIM_SetCompare1(HRTIM1, LL_HRTIM_TIMER_A, DEF_TMRA_STATIC_MAX_PWM_CTE-i_CalcDutyA);
LL_HRTIM_TIM_SetCompare3(HRTIM1, LL_HRTIM_TIMER_B, DEF_TMRA_STATIC_MAX_PWM_CTE+i_CalcDutyB);
LL_HRTIM_TIM_SetCompare1(HRTIM1, LL_HRTIM_TIMER_B, DEF_TMRA_STATIC_MAX_PWM_CTE-i_CalcDutyB);
//********* Optimized version **** 500ns or less
HRTIM1->sTimerxRegs[HRTIM_TIMERINDEX_TIMER_A].CMP3xR = DEF_TMRA_STATIC_MAX_PWM_CTE+i_CalcDutyA;
HRTIM1->sTimerxRegs[HRTIM_TIMERINDEX_TIMER_A].CMP1xR = DEF_TMRA_STATIC_MAX_PWM_CTE-i_CalcDutyA;
HRTIM1->sTimerxRegs[HRTIM_TIMERINDEX_TIMER_B].CMP3xR = DEF_TMRA_STATIC_MAX_PWM_CTE+i_CalcDutyB;
HRTIM1->sTimerxRegs[HRTIM_TIMERINDEX_TIMER_B].CMP1xR = DEF_TMRA_STATIC_MAX_PWM_CTE-i_CalcDutyB;
Now I'm looking for better/other optimization strategies (like writing Thumb/ARM assembly directly, as is already being done with mostly, if any, DSP that I've worked on), so the question is: how to do it in a correct way to mix with C/LL (C syntax) ? Any documentation available ?
(For example, a fastPID routine on this STM32F334 (72MHz) uses about 1000ns - 16bit Q15 fixed point arithmetic operations; on a dsPIC33 the same routine takes *only* 500ns - running at a theoretically lower clock speed - 40MIPs)
Thanks for any help.