Skip to main content
Graduate
October 14, 2021
Question

What's the worst that can happen if I assign a (quick) interrupt HIGHER prio than timer tick in FreeRTOS?

  • October 14, 2021
  • 3 replies
  • 1204 views

What's the worst that can happen if I assign an interrupt HIGHER prio than timer tick in FreeRTOS? Can I make the microcontroller or the operating system crash? The execution time of the high prio interrupt will be less than 100 microseconds and I plan to use 1 kHz tick frequency.

    This topic has been closed for replies.

    3 replies

    Super User
    October 14, 2021

    If that function doesn't touch anything important or shared, and if you have sufficient stack size, it should be invisible to the rest of the system.

    https://forums.freertos.org/t/systick-priority-vs-all-cortex-m-priorities/9289/2

    Except that it will introduce some jitter in SysTick and related things.

    Super User
    October 14, 2021

    The timer of FreeRTOS (usually the systick) can, and often has lower priority than other interrupts.

    There are also "quick" interrupts with priorities above configMAX_SYSCALL_INTERRUPT_PRIORITY. These interrupts are not blocked by RTOS activity.

    If you also want the ST "HAL" timer for the HAL library, you choose a normal timer (TIMx), give it a high priority and handle it as a "quick" interrupt.

    > Can I make the microcontroller or the operating system crash?

    Yes, always. Be careful.

    Graduate II
    October 14, 2021

    Yeah, both RTEMS and FreeRTOS need the tick timer to have the lowest priority in the system (if you look deep enough in the docs).

    I believe the idea is, when a tick interrupt happens, it doesn't merely increment the tick count, the ISR also goes through the task switch negotiations.

    You'll have to figure out what weirdness happens when one of your ISRs gets interrupted by the tick ISR and a task switch happens. It depends.

    arnold_wAuthor
    Graduate
    October 14, 2021

    I'm concerned about the oppsite, what will happen if the RTOS is in the middle of switching context from one thread to another and my high priority interrupt all of a sudden happens.

    Visitor II
    October 14, 2021

    Disregarding the CPU time, as long as the highest priority ISR does not access the RTOS API or your own hand-rolled semaphores/mutexes/etc., you should be OK. I've had to do this a couple times.

    FWIW, the ISR tracing functionality of your favorite IDE is your best friend right now. If you don't have one built in, use the SWO and a couple ITM channels; one for the RTOS task swap and one for your ISR. You can watch it happen and analyze the bananas out of it to convince yourself it's cool.