What should I do when the process stops in the middle of a program?
Hello everyone,
I am writing a program to read the gyro of the ICM42688P, but in the middle of the program, the process stops because it cannot be directed.
Here is the full text of the code↓
ICM42688P::ICM42688P(SPI_TypeDef *spi2, GPIO_TypeDef *cs_x, uint32_t cs_pin): spi2(spi2), cs_x(cs_x), cs_pin(cs_pin){}
void ICM42688P::setup(void){
LL_SPI_Enable(spi2);
}
void ICM42688P::SPI_TransmitReceive(uint8_t *tx_data, uint8_t *rx_data, uint8_t length) {
uint8_t count = length;
//CS Low
LL_GPIO_ResetOutputPin(cs_x,cs_pin);
//data clear
if (LL_SPI_IsActiveFlag_RXNE(spi2) == SET) LL_SPI_ReceiveData8(spi2);
//SPI、enable
if (LL_SPI_IsEnabled(spi2) == RESET) LL_SPI_Enable(spi2);
//sending receiving
while (count > 0) {
LL_SPI_TransmitData8(spi2, *tx_data++); //transmission
while (LL_SPI_IsActiveFlag_TXE(spi2) == RESET); //waiting transmission complete
while (LL_SPI_IsActiveFlag_RXNE(spi2) == RESET); //waiting reception complete
*rx_data++ = LL_SPI_ReceiveData8(spi2); //storage
count--;
}
//CS High
LL_GPIO_SetOutputPin(cs_x,cs_pin);
}
void ICM42688P::whoami() {
uint8_t tx_data[2];
uint8_t rx_data[2];
//who_am_i read
tx_data[0] = (0x75 | 0x80); //read
tx_data[1] = 0x00; //dummy
SPI_TransmitReceive(tx_data, rx_data, 2);
printf("who am i = %x\r\n", rx_data[1]);
}
The process stops in the following part↓
while (LL_SPI_IsActiveFlag_TXE(spi2) == RESET);
while (LL_SPI_IsActiveFlag_RXNE(spi2) == RESET);
However, if this part is deleted, the process will not stop but will not return the value expected by whoami.
Is there any good solution?
Thank you in advance.
microcontroller stm32f407vgt6, cubeIDE