Question
What STM32 development boards support developing with a High Speed USB device?
It should use a chip with low pincount/small package.
I need to connect a UART an SPI and a few GPIOs.
Even chips with HS USB seems to only support FS USB on the development boards I looked at. While the chip does not use too much bandwidth, there are other high bandwidth devices
on the bus, and HS USB Is needed for everything or everything else will slow down.