Skip to main content
Visitor II
September 11, 2023
Question

When configuring STM32F107RC FreeRTOS, the interrupt CALLBACK function is not called

  • September 11, 2023
  • 0 replies
  • 528 views


Hello.

I have some questions while testing a product using the 107MCU.

As the title suggests, when I set up FreeRTOS and create a task, the commonly used callback functions cannot be called:

void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

If I remove the task creation function, it operates normally.

Do you know why this is happening?

Thank you.

    This topic has been closed for replies.