Skip to main content
Visitor II
December 6, 2021
Question

Which class of USB is used for making the communication between the STM and Application ?

  • December 6, 2021
  • 0 replies
  • 473 views

Helllo,

I am working on Nucleo-h745ziq board. Using the GUI I creating the application of 3 LED and one user button. When I press the switch the led starts the blinking on stm32,For this purpose which Usb class that I have use HID or Custome HId. Can you please help me. If there is example like that in cubemx can you suggest me.

    This topic has been closed for replies.