Why do I get "ERROR with Trace_" errors from the USB-C stack in STM32CubeMonitor?
Hi,
lately I realized that there are tracer errors from the USB-C stack in STM32CubeMonitor. I haven't seen them with older version of the USBPD libraries.
Currently I'm using:
- FW pack STM32Cube_FW_G0_V1.5.1
- USBPD core library is now V4.0.0
- USBPD device library is now V3.3.1
Where do these errors come from?
Thanks!
BR, Christoph