Why does the HAL USB CDC driver call malloc in an ISR context?
Since __malloc_lock has not been implemented by default, newlib's malloc / _malloc_r is not reentrant or thread safe (including ISR safe). This seems like a bug.
This will cause very bad interactions with user code use of malloc, including heap corruption. Additionally, most RTOS's heaps are not ISR-safe, so when using the freertos heap it causes a crash. Usually when using newlib & freertos I implement _mallor_r to use the rots heap, and provide __malloc_lock and __malloc_unlock so it is threadsafe. This is necessary so the C library internal allocations are threadsafe, but doing so causes a crash when the cdc driver attempts to allocate memory within the ISR.
Can this be changed to allow either a statically allocated buffer, a user provided buffer, or a thread-context dynamically allocated buffer? I have moved the classData it is trying to allocate to be static for now, but in general this needs to be allocated per usb instance, so a single one is not enough.
Perhaps a user provided buffer passed in at configuration time would be better.