Skip to main content
Visitor II
February 16, 2021
Solved

Why is there no implementation of Low Level drivers for MDMA on STM32H7xx.

  • February 16, 2021
  • 2 replies
  • 926 views

Hi all,

I have a project for which we need as fast as possible drivers so we use as much as possible the LL drivers . Yet it seems that there was no implementation of LL for MDMA, even if it seems that all other DMA managers have theirs.

Anyone knows why it is the case?

And also do you know if there will be a future implementation of these drivers?

Thanks

Seb

    This topic has been closed for replies.
    Best answer by Imen.D

    Hello @SGuic.1​ and welcome to the STM32 Community,

    The LL MDMA driver is already integrated in the STM32CubeH7 MCU package.

    You will find the stm32h7xx_ll_mdma files in the following driver paths:

    • stm32h7xx_ll_mdma.c under the STM32Cube_FW_H7_V1.8.0\Drivers\STM32H7xx_HAL_Driver\Src
    • stm32h7xx_ll_mdma.h files, in the STM32Cube_FW_H7_V1.8.0\Drivers\STM32H7xx_HAL_Driver\Inc

    If you mean the implementation in the STM32CubeMx tool: It is planned to integrate the LL MDMA driver in the future, but I can't give you any target date for the moment.

    Please mark my answer as best by clicking on the "Select as Best" button if it fully answered your question. This can be very helpful for Community users to find this answer more quickly.

    Imen

    2 replies

    Imen.DAnswer
    Technical Moderator
    February 16, 2021

    Hello @SGuic.1​ and welcome to the STM32 Community,

    The LL MDMA driver is already integrated in the STM32CubeH7 MCU package.

    You will find the stm32h7xx_ll_mdma files in the following driver paths:

    • stm32h7xx_ll_mdma.c under the STM32Cube_FW_H7_V1.8.0\Drivers\STM32H7xx_HAL_Driver\Src
    • stm32h7xx_ll_mdma.h files, in the STM32Cube_FW_H7_V1.8.0\Drivers\STM32H7xx_HAL_Driver\Inc

    If you mean the implementation in the STM32CubeMx tool: It is planned to integrate the LL MDMA driver in the future, but I can't give you any target date for the moment.

    Please mark my answer as best by clicking on the "Select as Best" button if it fully answered your question. This can be very helpful for Community users to find this answer more quickly.

    Imen

    SGuic.1Author
    Visitor II
    February 16, 2021

    Okay perfect.

    Was just strange that the STM32CubeIDE wasn't proposing the option.

    I'll just manually add them and I'll be all good.

    Thanks a lot.

    Seb