Why use DMA when you've got shared RAM?
I've inherited some code, the original owner is long gone, and I'm trying to understand his code which has ZERO comments (I'm sure I'm not the only person who's been in this position)
It's using the STM32H747IGT6 so it's dual core, got one M4 and one M7 core. They are using SRAM2 to communicate, but he's got it set up so the M4 (which is generating the data) writes a single uint32 of data into one location in SRAM2 and then triggers the MDMA to move it to another location in SRAM2 where the M7 can pick it up.
I haven't worked with a dual-core STM32 before, but this feels like overkill. If both cores can read & write SRAM2, why bother with the MDMA? Why not just have the M4 write the data directly to where the M7 will be looking for it and skip the MDMA completely?
And why is he setting the destination bus to AXI (and leaving the source bus at is default of AXI) when the system architecture diagram shows SRAM2 as being in the AHB bus matrix? I'm thinking that since SRAM2 is mapped at the same address in both bus systems, it doesn't actually matter which bus is selected?
Here is his MDMA initialization code, I've started writing comments to explain each step:
/*
* Set MDMA first channel BNDT (in MDMA_CxBNDTR) to transfer sizeof(uint32_t) * SHMEM_NUM_SAMPLES bytes
* "Number of bytes to be transferred (0 up to 65536) in the current block. When the channel is
* enabled, this register is read-only, indicating the remaining data items to be transmitted.
* During the channel activity, this register decrements, indicating the number of data items
* remaining in the current block.
* Once the block transfer has completed, this register can either stay at zero or be reloaded
* automatically with the previously programmed value if the channel is configured in block
* repeat mode."
* #define SHMEM_NUM_SAMPLES 4096
*/
LL_MDMA_SetBlkDataLength(MDMA, LL_MDMA_CHANNEL_0, sizeof(uint32_t) * SHMEM_NUM_SAMPLES);
/*
* Set MDMA first channel BRC (in MDMA_CxBNDTR) to zero
* "This field contains the number of repetitions of the current block (0 to 4095). When the
* channel is enabled, this register is read-only, indicating the remaining number of blocks,
* excluding the current one. This register decrements after each complete block transfer.
* Once the last block transfer has completed, this register can either stay at zero or be
* reloaded automatically from memory (in linked-list mode, meaning link address valid)."
* I think this is set to "not repeat" so that the buffer will wait until the CM7 can grab
* it before it starts a new pass. See LCSCM7BSPReleaseSharedData().
*/
LL_MDMA_SetBlkRepeatCount(MDMA, LL_MDMA_CHANNEL_0, 0);
/*
* Set MDMA first channel BRDUM (in MDMA_CxBNDRT) to zero
* "At the end of a block transfer, the MDMA_DAR register is updated by adding the DUV to
* the current DAR value (current destination address)."
*/
LL_MDMA_SetBlkRepeatDestAddrUpdate(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_BLK_RPT_DEST_ADDR_INCREMENT);
/*
* Set MDMA first channel BRSUM (in MDMA_CxBNDRT) to zero
* "At the end of a block transfer, the MDMA_SAR register is updated by adding the SUV to
* the current SAR value (current source address)."
*/
LL_MDMA_SetBlkRepeatSrcAddrUpdate(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_BLK_RPT_SRC_ADDR_INCREMENT);
/*
* Set MDMA first channel DUV (Destination address update value) (in MDMA_CxBRUR) to 4
* "This value is used to update (by addition or subtraction) the current destination address at the end of
* a block transfer."
*/
LL_MDMA_SetBlkRptDestAddrUpdateValue(MDMA, LL_MDMA_CHANNEL_0, 4);
LL_MDMA_SetBlkRptSrcAddrUpdateValue(MDMA, LL_MDMA_CHANNEL_0, 0);
/*
* Set MDMA first channel TLEN (buffer transfer length, in MDMA_CxTCR) to 3
* "TLEN + 1 value represents the number of bytes
* to be transferred in a single transfer."
*/
LL_MDMA_SetBufferTransferLength(MDMA, LL_MDMA_CHANNEL_0, 3);
LL_MDMA_SetByteEndianness(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_BYTE_ENDIANNESS_PRESERVE);
LL_MDMA_SetChannelPriorityLevel(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_PRIORITY_HIGH);
/*
* Set MDMA first channel DBUS (Destination bus select, in MDMA_CxTBR) to zero
* "The system/AXI bus is used as destination (write operation)"
*/
LL_MDMA_SetDestBusSelection(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_BUS_SYSTEM_AXI);
/*
* Set MDMA first channel CDAR (channel destination address register, in MDMA_CxDAR)
* to &shared_mem[SHMEM_SAMPLE_0_INDEX]
* #define SHMEM_SAMPLE_0_INDEX 256
*/
LL_MDMA_SetDestinationAddress(MDMA, LL_MDMA_CHANNEL_0, (uint32_t)&shared_mem[SHMEM_SAMPLE_0_INDEX]);
LL_MDMA_SetDestinationBurstSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_BURST_SINGLE);
LL_MDMA_SetDestinationDataSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_DATA_SIZE_WORD);
LL_MDMA_SetDestinationIncMode(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_INCREMENT);
LL_MDMA_SetDestinationIncSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_DEST_INC_OFFSET_WORD);
/*
* SET MDMA first channel CSAR (source address, in MDMA_CxSAR) to &shared_mem[SHMEM_PIPE_LAUNCH_INDEX]
* #define SHMEM_PIPE_LAUNCH_INDEX (LCS_SHARED_MEM_LEN - 1)
*/
LL_MDMA_SetSourceAddress(MDMA,
LL_MDMA_CHANNEL_0,
(uint32_t)&shared_mem[SHMEM_PIPE_LAUNCH_INDEX]);
LL_MDMA_SetSourceBurstSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_SRC_BURST_SINGLE);
LL_MDMA_SetSourceDataSize(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_SRC_DATA_SIZE_WORD);
/*
* Set MDMA first channel SINC (source increment mode) (in MDMA_CxTCR) to zero
* "Source address pointer is fixed."
*/
LL_MDMA_SetSourceIncMode(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_SRC_FIXED);
/*
* Set the SWRM (software request mode) (in MDMA_CxTCR) to 1
* "Hardware request are ignored. Transfer is triggered by software writing 1 to the SWRQ bit."
*/
LL_MDMA_SetRequestMode(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_REQUEST_MODE_SW);
/*
* Set the TRGM (trigger mode) (in MDMA_CxTCR) to zero
* "Each MDMA request (software or hardware) triggers a buffer transfer."
* Above, we set TLEN to 3 so 4 bytes are sent each time a request is triggered
*/
LL_MDMA_SetTriggerMode(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_BUFFER_TRANSFER);
// LL_MDMA_SetHWTrigger(MDMA, LL_MDMA_CHANNEL_0, LL_MDMA_REQ_DMA1_STREAM0_TC);
LL_MDMA_EnableIT_CTC(MDMA, LL_MDMA_CHANNEL_0);
LL_MDMA_EnableChannel(MDMA, LL_MDMA_CHANNEL_0);