Why would the NxWebServer example stop firing the webserver_request_notify_callback?
I have ported the NxWebServer example from the STM32H735-DK project over to the STM32H743i-eval. All the bugs seem to be worked out and connection is being made. I can see get requests coming in to the call back but after the second or third file for the main webpage the callbacks stop.
I have tried slowing the SDMMC clock, Disabling Cache, to no avail. I have tried using the debugger to pause the code when the callbacks stop and the the code is always in the RTOS idle state with all the tasks either suspended or completed with the exception of the remaining sleeping thread that checks for connection status once every 10 seconds. On occation I will get the whole web page but that is very rare.
Not sure where else to look.