wierd behavior of ETH on STM32H7
I am trying to set up ethernet on stm32h745iit6.
I bare ethernet project from the H7 examples and use (low_level_output) func from ethernetif.cpp.
I send buffer, located 0x24000008, where dma can access. And ethernet always send only init string of buffer. When I try to change content of the buf from code, its changes (as i saw in debug) at location 0x24000008. But in wireshark i still recieving init content of the value (string, that no longer exist).
When i change content of the buffer from debug at the same location, its ok and recieve correct string with all changes, that was made in debug.
Also a watch on the descriptor field DESC0, there 0x24000008, where located my buf.
Is there any explanation of this wierd moment? How i should change content of buf so that it works correctly ? Maybe data cashes somewere in DMA or MTL?