With the STM32F417VGT6 chip used, after PA11 PA12 is configured as USB HOST (non-OTG mode, HNP or SRP mode is not used), PA9 cannot be configured as input pull-up mode.
After using STM32F417VGT6 chip, PA11 PA12 is configured as USB HOST (non-OTG mode, HNP or SRP mode is not used), PA9 cannot be configured as input pull-up mode; without USB HOST, PA9 can be configured as input pull-up Yes; try to configure PA9 to output pull-up or serial port can be used normally; configure PA9 to input pull-up mode, without connecting any peripherals, measure PA9 pin as low level. When using PA11 PA12 USB HOST, do you configure PA9 as input pull-up?