x-cube AWS OTA fails (Solved)
Hello geeks....
I'm using x-cube aws sdk with P-L496G-CELLONE development board
SDK version is 1.4.0 having aws version 3.0.1
I can successful connect with the my MQTT aws server
Now the problem is, when i try to do OTA then, out of 5 attempts, 4 attempts fails
Every time I'm getting same errors of handshaking(-0x2700)
I have all default settings in mbedtls_config.h
I'm unable to set the debug_level to 4 due to the limitations of the SRAM in mbedTLS
Here is the error logs

All suggestions and comments welcome
Thanks