Skip to main content
Visitor II
January 7, 2026
Question

X-CUBE-EEPROM: writing stops when both pages full; data no longer read correctly.

  • January 7, 2026
  • 0 replies
  • 48 views

I'm using the X-CUBE-EEPROM library on my STM32C031G6Ux to store keys in flash memory. I configured eeprom_emul_conf.h so that the emulated EEPROM starts at 0x08007000, with 2 pages of 2 KB each, and set NB_OF_VARIABLES to 240.

When I tried saving 240 variables once using EE_WriteVariable32bits and reading them back with EE_ReadVariable8bits, everything worked fine.

However, when I repeat this process three times, writing stops once both pages are full, and the data is no longer read correctly.

I experienced similar issues even with 120 variables. Interestingly, adding EE_CleanUp after all writes solved the problem for 120 variables.

I then tried the same approach with 240 variables, calling EE_CleanUp after all write operations, but it still didn’t work.

Is there a reason for this behavior? Am I limited to storing only 120 variables in flash?

    This topic has been closed for replies.