X-CUBE-USB-PD problem, stopped responding to anything after I unplugged the cable.
The X-CUBE-USB-PD is running on my custom PCB with the STM32F072CB and FUSB307B. That project is based on the sample project, EVAL_FUSB307B_DRP, which works as a DRP.
When I have traces functioning at build time and the system is acting as a source, if I pull the plug, the program may not respond to anything after that.
Pulling the plug when the trace is off and when the system is acting as a sink will not cause any problems.
The last I2C communication record.
Immediately after an attempt to access the 0x70(VBUS_VOLTAGE_L) register, the system stops responding.The alert has been on LOW ever since.