Skip to main content
Visitor II
February 25, 2024
Question

X-NUCLEO-IDW01M1 plus NUCLEO-H753ZI Wifi Stack ?

  • February 25, 2024
  • 1 reply
  • 995 views

Hi, 

 

if i combine 

X-NUCLEO-IDW01M1

NUCLEO-H753ZI

 

does the WIFI plug in as a 2nd netif in lwip in the H753 ? 

 

or is it like 2 Microcontrollers just connected to each other and the App Developer is on its own ? 

 

how does it compare to the 

AIROC™ Wi-Fi/Bluetooth® STM32 expansion pack from Infineon ? 

 

which one has the better Software Stacks ? 

 

I am interested in a as much as possible transparent adaption to Wifi over 

STM32CubeIDE project with lwIP + FreeRTOS

Thanks. 

 

    This topic has been closed for replies.

    1 reply

    ST Employee
    June 7, 2024

    Hello @franzhoepfinger,

     

    When you combine the X-NUCLEO-IDW01M1 Wi-Fi module with the NUCLEO-H753ZI board, the Wi-Fi module can indeed be configured as a secondary network interface (netif) in the lwIP stack on the H753ZI. It's not merely a connection between two microcontrollers; the module is designed to integrate with the STM32 ecosystem and lwIP.

    Comparing it to Infineon's AIROC™ Wi-Fi/Bluetooth® STM32 expansion pack, the latter offers additional Bluetooth functionality, which might be beneficial if you require both Wi-Fi and Bluetooth for your project. As for software stacks, both are well-supported within their respective ecosystems, but the best choice depends on your specific needs and whether Bluetooth capability is a requirement.

    The X-NUCLEO-IDW01M1 aims for a straightforward and transparent adaptation to Wi-Fi, making it a great choice if Wi-Fi connectivity is your primary concern.

    With Regards,