Zephyr with STM32H735g_disco board crashes when executing the z_msleep function
Project: samples/basic/blinky
board: stm32h735g_disco
I am using the latest Zephyr 4.1
If have a simple project `sample/basic/blinky`. Using the west command to compile the project, flash the board, debug the board with OpenOCD protocol.
Everytime I used the debugger (dbg), I am able to step by step the project until I reach the k_msSeep() function.
A friend of mine help me to debug it and we were able find that the system breaks as indicated in the picture below.
If I don't use the debugger DBG, then the software does not crash... It just work.