STEVAL-SPIN3202. Got it turning. Now need a guidance on where / what file and how I can control the speed.
Hi All,
Got it turning. Now need a guidance on where / what file and how I can control the speed.
SDK 5.4.8.
6S_STEVAL3202_SL_VM example.
Monitor connects well.
I can start the motor.
Final ramp speed does not work. The only use - setting the direction of rotation.
Measured speed raises from 0 to 4000rpm and motor stops with Fault over "Start-up failure". Motor power indicator jumps to max and stays there.
My application is simple. I need an open loop control. 2 speeds forward, 2 speeds reverse. Stop. Preferably hardware control -3 pin. The only feedback - hardware Fault output.
Questions are:
- Where (what settings) can be an error.
- Where can I find the code where I can control the speed.
- How I can control the speed (what variables are responsible for speed and acceleration?). I assume that it can be done in main.c in while(1) loop.
- Could you please direct me to some manual or documentation on 6S_STEVAL3202_SL_VM package.
Thanks in advance for your answers.
Regards,
Edward.