Skip to main content
OGhis
Senior
July 31, 2024
Solved

2 QSPI RAM on STM32H7B0 with APS6404L-3SQN-SN

  • July 31, 2024
  • 4 replies
  • 1421 views

Dear,

We would on the STM32H7B0RBTx connecting 2 external QSPI RAM of APS6404L-3SQN-SN.
Therefore we will use the 2 QSPI RAM chips in Multiplex mode, but we have only 1 NCS pin that we can configure.
When we look in the application note AN5050 on page 27 we see that it is possible but with STM32Cube it isn't possible to configure the NCS pin on port 2.

OGhis_0-1722421226713.png

What we doing wrong here?

How we should configure the other parameters of the QCTOSPI in STM32cube for the used RAM chip?
OCTOSPI1

OGhis_1-1722422470333.png

OCTOSPI2:

OGhis_2-1722422511544.png



Best answer by KDJEM.1

Hello @OGhis ,

For the STM32H7B0RBTx, the multiplexed mode is not supported because the OCTOSPIM_P2_NCS pin isn’t available.

the Multiplexed mode requires BOTH OCTOSPIM_P2_NCS AND OCTOSPIM_P1_NCS as mentioned in the RM0455 and in AN5050. 

KDJEM1_1-1722432349068.png

 

KDJEM1_0-1722432318247.png

May this discussion can help you.

I confirm the issue in STM32CubeMx and I reported internally.

Internal ticket number: 187830 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

 

4 replies

TDK
Super User
July 31, 2024

The OCTOSPIM_P2_NCS pin is PG12 which isn't available on the LQFP64 package.

TDK_0-1722430189786.png

 

STM32H7B0RBTx is an LQFP64 package, rather small, so it has a limited number of pins. You'll have to move up to a larger package, at least the LQFP144, if you want to do this.

"If you feel a post has answered your question, please click ""Accept as Solution""."
KDJEM.1
KDJEM.1Best answer
Technical Moderator
July 31, 2024

Hello @OGhis ,

For the STM32H7B0RBTx, the multiplexed mode is not supported because the OCTOSPIM_P2_NCS pin isn’t available.

the Multiplexed mode requires BOTH OCTOSPIM_P2_NCS AND OCTOSPIM_P1_NCS as mentioned in the RM0455 and in AN5050. 

KDJEM1_1-1722432349068.png

 

KDJEM1_0-1722432318247.png

May this discussion can help you.

I confirm the issue in STM32CubeMx and I reported internally.

Internal ticket number: 187830 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
OGhis
OGhisAuthor
Senior
August 1, 2024

Thanks
We have switch the MCU to a 144 pins and now we can configure the 2 QSPI.

Can we have also an answer on my second question?
==> How we should configure the other parameters of the QCTOSPI in STM32cube for the used RAM chip? (see first message)

KDJEM.1
Technical Moderator
August 1, 2024

Hello @OGhis ,

 

Could you please refer to AN5050 "Table 7. STM32CubeMX - Configuration of OCTOSPI signals and mode" and "Table 8. STM32CubeMX - Configuration of OCTOSPI parameters" and get inspired to configure two QSPI RAM in multiplexed mode.

These two tables give some examples of OCTOSPI configurations. 

I hope this help you.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KDJEM.1
Technical Moderator
July 10, 2025

Hello @OGhis;

 

The STM32CubeMX issue is resolved in STM32CubeMX version 6.15.0

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.