A question about the UART irq code generate by cubemx
When a USART is configured without a clock, the code generator treats it as a UART and assigns HAL_UART_IRQHandler as the interrupt handler. However, within this handler, there is a blocking operation during the idle process:(void)HAL_DMA_Abort(huart->hdmarx);
When certain error conditions occur, the code can become stuck in HAL_GetTick(). This happens because the SysTick priority is lower than that of the UART interrupt. I have observed this behavior multiple times, particularly when noise is present on the UART signal line.
Has Anyone seen this situation before?